Technical FAQs

Ask a Question

How to access emergency stop remotely when Altivar 312 drive operation is performed from LOCAL.

To have remote access on Altivar 312 drive even when drive operation is performed from LOCAL, use
Forced Local Mode of drive. With Forced Local Mode of drive, drive is made operational from LOCAL
only when Forced Local command is activated from remote. As soon as Forced Local Command is
deactivated from remote, drive will stop according to STT (Stop type) assign.
 
Was this helpful?
What can we do to improve the information ?