Technical FAQs

Ask a Question

How to overcome problem of connection lost in serial communication while making use of SoMove Lite with PC.

In Case of “Connection Lost” when using Serial Communication, configure the Inter-Char Timeout from the Modbus Driver as follows:
 
1. Select the Modbus driver from the taskbar. The default settings for Inter-Char Timeout will be automatic.
2. Select the COM Port to be used and change the Inter-Char Timeout value to higher value. eg. 50 ms.



Was this helpful?
What can we do to improve the information ?