Technical FAQs

Ask a Question

Can we change the controller model in a existing SoMachine application.

Controller in the SoMachine application can be changed from the SoMachine version 3.1 onwards. But only the
controller can be changed within the same family of controller. For example if you want to change the controller from
M218 family (TM218LDA16DRN) to M238 or M258 it is not possible you can only change the M218 (TM218LDA16DRN)
to another model of M218 family (TM218LDA24DRHN).
To change the controller type right click on the controller from object browser of the SoMachine software and click on
Change Device. Select the controller you wish to change and press on Change Device button. It will the update your application
according to the controller you have selected.
Was this helpful?
What can we do to improve the information ?