Technical FAQs

Ask a Question

Is it possible to change the font size of the Alarm Page during runtime.

You can do this with help of AlarmSetInfo() function. You have to write a cicode with help of using this function to change
the alarm fonts during runtime.
For example, if you have a button which has the following cicode function as its input:
FUNCTION FmtAlarmDsp()
INT hFont;
      hFont = DspFont("Arial",-11,black,grey);
      AlarmSetInfo(-1, 6, hFont);
Was this helpful?
What can we do to improve the information ?