Technical FAQs

Ask a Question

Can we install "Vijeo Citect" and "Vijeo Historian" in same PC and run both of them.

There is no problem if you install and use Vijeo Citect and Vijeo Historian on a same system. But only thing that you
would have to consider is that both the licenses of Vijeo Citect and Vijeo Historian should be merged on a single key.
because it may create problem in license detection if both were having different license key and you would insert two
seperate license for them.
Was this helpful?
What can we do to improve the information ?