Technical FAQs

Ask a Question

I am using Vijeo Citect V7.2 in that group trend is not available, I want to configure the same trend groups as like of Vijeo Citect V7.1

You can configure Trend Group in Vijeo Citect V 7.20 also. It`s simple and easy to use in V 7.20 but for that you have to first add
 the "CSV_Include" project in your project directory and then include it in your project also by this
path -->> Go to Citect Project Editor >> System >> Included Projects >> write CSV_Include in project name and then press add button.
After that you can configure trend group in the "TrendGrp.dbf" file, which you will found in the [RUN] directory of Citect.
Was this helpful?
What can we do to improve the information ?