Technical FAQs

Ask a Question

What is the Power dissipation for CT contactors according to different ratings.

The Power dissipation for CT contactors according to different ratings are
 
16A  =  0.65W
25A  =  1.65W
40A  =  1.65W
63A  =  1.65W
100A =  1.65W
Was this helpful?
What can we do to improve the information ?