Technical FAQs

Ask a Question

What is the difference between the LUCA32** and the LUCB32**?

The LUCA32 is a standard control module that provides 3 phase, class 10, solid state overload relay protection along with the coil circuit. When the starter is also equipped with a communications module, the LUCA32 can accept run commands via the network.

The LUCB32 is an advanced control module and also provides 3 phase, class 10,  solid state overload relay protection and control coil but  also provides additional data via the network communication module.


CTA-ID : 2061136
Was this helpful?
What can we do to improve the information ?