Technical FAQs

Ask a Question

DF103: what type of fuse do these holders accept?

The fuseholders accept aM cartridge fuses refer to Catalog 9080CT0801page 6.
The fuse size is mm 10 x 38 and (Inch) (0.4 x 1.5). They are rated the same as CC fuses.

CTA-ID : 2061434
Was this helpful?
What can we do to improve the information ?