Technical FAQs

Ask a Question

What is Rated impulse-withstand voltage (Uimp) for Circuit-breakers.

This characteristic expresses, in kV peak, the value of voltage which the equipment is capable of withstanding
 without failure, under test conditions.
Generally, for industrial circuit-breakers, Uimp = 8 kV and for domestic types, Uimp = 6 kV.
Was this helpful?
What can we do to improve the information ?