Technical FAQs

Ask a Question

Can the ATV312 be powered by an external 24V only?

No, this drive must have line voltage applied.  The voltage must be within -15% to +10% of the rated line voltage.  


CTA-ID : 2061616
Was this helpful?
What can we do to improve the information ?