Technical FAQs

Ask a Question

How many Modbus slaves can be configured with one LUFP7 Profibus-DP to Modbus RTU gateway.

Each LUFP7 Profibus-DP / Modbus RTU gateway allows one of the PLCs on the Profibus-DP
network to command, control and configure up to 8 Modbus slaves.
Was this helpful?
What can we do to improve the information ?