Technical FAQs

Ask a Question

What is the addressing range for encoding the LUFP7 gateway.

The LUFP7 gateway is identified on the Profibus-DP bus by its address, ranging from 1 to 99.
 
The gateway's Profibus-DP address depends on the position of the two coding wheels represented on the
left, in their factory-setting positions (default address = 2).
 
This address is the sum of the decimal values given by the angular positions of the bottom coding wheel (tens) and
the top coding wheel (units).
 
 
Was this helpful?
What can we do to improve the information ?