Technical FAQs

Ask a Question

What is the level of vacuum pressure inside the Evolis circuit breaker.

The vacuum level inside the vacuum bottle is 10-2 Pa.
Was this helpful?
What can we do to improve the information ?