Technical FAQs

Ask a Question

What is the class of the Evolis Circuit breaker in terms of mechanical endurance and what is the value for this.

As per IEC 62271, the mechanical endurance class of the Evolis circuit breaker is class M2 except

Evolis 240 mm: Class M1
Evolis 185 mm 40 kA only: Class M1.
 
Class M2 means the total no. of operation is 10000.
Class M1 means the total no. of operation is  2000.
Was this helpful?
What can we do to improve the information ?