Technical FAQs

Ask a Question

What is the operating temperature of Evolis circuit breaker and is there any temperature derating possible beyond the operating limit.

The operating temperature of the Evolis is -25*C to 40*C.
The temperature derating is 1% Ir per degree above 40°C.
Was this helpful?
What can we do to improve the information ?