Technical FAQs

Ask a Question

What is the power frequency withstand voltage of the Evolis circuit breaker.

The Power frequency withstand voltage for Evolis VCB as per the rated voltage is as below

Rated Voltage (kV) Power frequency withstand (kV)
7.2 20
12 28
17.5 38
Was this helpful?
What can we do to improve the information ?