Technical FAQs

Ask a Question

What is the SF6 gas pressure & weight values used in LF range of circuit breaker.

The SF6 gas pressure values used in LF range of circuit breaker is 1.5 bar and the weight is as below.

  LF1 LF2 LF3 LFP
SF6 Gas Weight ( g ) 399 461 614 783
Was this helpful?
What can we do to improve the information ?