Technical FAQs

Ask a Question

What is the maximum possible distance between FDM121 display unit and Compact NSX circuit breaker.

The maximum recommended distance between FDM and Compact NSX or IFM module is 10 meter.
You can prolong the cable by TRV00870, or can try to make a longer cable with correct crimping of connectors but max. 10m.
Was this helpful?
What can we do to improve the information ?