Technical FAQs

Ask a Question

What is the IP value for FDM121 display unit of Compact NSX breaker.

The FDM121 degree of protection is IP54 in front.
IP54 is maintained after switchboard mounting by using the supplied gasket during installation.
Was this helpful?
What can we do to improve the information ?