Technical FAQs

Ask a Question

What are the differences between a Reflex iC60 integrated control circuit breakers and a RCA remote control.

The Reflex iC60 is a circuit breaker with an integrated control unit designed exclusively for remote opening/closing control
and is sized to allow a large number of switching operations.
 
The RCA remote control is a circuit breaker auxiliary which allows remote opening and closing and automatic reclosing upon a
fault. The electrical endurance of the remote control is limited by the endurance of the circuit breaker that is associated with it.

Was this helpful?
What can we do to improve the information ?