Technical FAQs

Ask a Question

What is the service life of the Reflex iC60 integrated control circuit breakers.

The mechanical endurance of the Reflex iC60 is 50,000 switching cycles (O/C).
The electrical endurance varies depending on the use and loads (rating, derating, class of use, pf).
Was this helpful?
What can we do to improve the information ?