Technical FAQs

Ask a Question

What are the advantages of the bistable operation of the Reflex iC60 integrated control circuit breakers.

Due to its bistable operation, the Reflex iC60 does not require maintenance of the power supply for
control orders, and it has the following advantages:
 
- Improved continuity of service because the outgoing feeder remains powered even in the event of loss of
  the control power;
 
- Environmentally friendly due to almost zero power consumption by the product in steady-state conditions
  and less unwanted temperature rise.
Was this helpful?
What can we do to improve the information ?