Technical FAQs

Ask a Question

Is the Reflex iC60 integrated control circuit breakers compatible with a resistive heating application.

The Reflex iC60 is compatible with AC1 type applications (resistive heating circuit). However, in the case of a
heating system with regulation, it should be ensured that the number of controls and the switching rate are compatible
with the performance limits of the Reflex iC60 in order to guarantee its robustness.
Was this helpful?
What can we do to improve the information ?