Technical FAQs

Ask a Question

What types of loads can be controlled with the Reflex iC60 integrated control circuit breakers.

Loads having the following classes of use can be controlled with the Reflex iC60:
 
AC5b: Incandescent and halogen lamps.
 
AC5a & AC7c: Discharge lamps (fluorescent tubes, sodium vapour, LED, etc.)
 
AC1, AC7a: Electric heating appliances, water heaters, ovens.
 
AC7b: Motors for domestic applications.
Was this helpful?
What can we do to improve the information ?