Technical FAQs

Ask a Question

Is the Reflex iC60 integrated control circuit breakers compatible with auxiliaries and accessories.

The Reflex iC60 is not compatible with the indication auxiliaries of the Acti 9 range (iOF, iSD, iSD+OF, iMX, iMX + OF, iMN,iMNs, iMNx).
The Reflex iC60 incorporates O/C and Auto/OFF auxiliary indication contacts which allows user to know remotely the status of the circuit
breaker and contacts.
The Reflex iC60 can be associated with an iC60 Vigi module.
iOF : open/close auxiliary contact
iSD : fault indicating contact
iMX,iMX+OF : shunt release , shunt release + auxiliary contact
iMN : under voltage release
iMNs: under voltage release delayed
iMNx: under voltage release with external feeding
Was this helpful?
What can we do to improve the information ?