Technical FAQs

Ask a Question

What are the inputs (Y1, Y2 and Y3) in Reflex iC60 integrated control circuit breakers.

Y1 is a 230 Vac latched type control.
Y2 is a 230 Vac impulse type control.
Y3 is a 24 Vdc latched type control.
Was this helpful?
What can we do to improve the information ?