Technical FAQs

Ask a Question

What is the purpose of the Ti24 interface in Reflex iC60 integrated control circuit breakers and the control voltage via it.

The Ti24 interface allows direct connection of the Reflex iC60 with 24 Vdc input/output interfaces, e.g. a programmable logic controller.
The Ti24 interface is a 24 V input/output interface.
Was this helpful?
What can we do to improve the information ?