Technical FAQs

Ask a Question

What is the default Mode of the Reflex iC60 integrated control circuit breakers.

On versions without the Ti24 interface, the default mode of the Reflex is Mode 1.
 
On versions with the Ti24 interface, the default mode of the Reflex is Mode 3.
 
The Ti24 interface allows direct connection of the Reflex iC60 with
24 Vdc input/output interfaces, e.g. a programmable logic controller.
 
Was this helpful?
What can we do to improve the information ?