Technical FAQs

Ask a Question

Is it possible to know locally which is the selected mode in reflex iC60 integrated control circuit breakers.

When the Reflex operating handle is in closed position, the number of flashes of the indicator on the front
panel indicates the operating mode of the Reflex iC60: one flash corresponds to Mode 1, two flashes at a
short interval correspond to Mode 2 and three flashes at a short interval correspond to Mode 3.
Was this helpful?
What can we do to improve the information ?