Technical FAQs

Ask a Question

What is the noise level of Altivar 212 range.

The power part of the Altivar 212 is the same as Altivar 21.So, the noise level of Altivar 212 range is same as Altivar 21.
Refer to attached file for noise level of Altivar 212 range.
Was this helpful?
What can we do to improve the information ?