Technical FAQs

Ask a Question

Is any communication port in-built in Altivar 303.

Altivar 303 has integrated Modbus Communication protocol which can be accessed via RJ 45 connector.
 
Was this helpful?
What can we do to improve the information ?