Technical FAQs

Ask a Question

Is Altivar 303 confirms the standard IEC 61800-3.

Yes, Altivar 303 confirms the standard IEC 61800-3.
Refer to attached file for manufacturer's declaration report of Altivar 303 drive.
Was this helpful?
What can we do to improve the information ?