Technical FAQs

Ask a Question

What is the number of Input/Outputs with Altivar 303 drive.

Altivar 303 has following Input/Outout. 

1 Analog Input Programmable as 0-5/10V or 0-20mA
1 Analog Output 0-10V or 0-20mA
4 Logic Input
1 Logic Output
1 Relay Output with 2 change over
Was this helpful?
What can we do to improve the information ?