Technical FAQs

Ask a Question

Vijeo Citect Express Wizard not working when used with VJC 7.10 SP1.

On PC`s where no serial ports exist, the express wizard would go into a indefinite loop. This issue has been addressed in the latest Service Pack SP4
or else you can use a device ( like TSXCUSB485 ) which creates a virtual com port.
Was this helpful?
What can we do to improve the information ?