Technical FAQs

Ask a Question

I want to view a notepad file in runtime for viewing events logs, so what is the maximum file size that I can open using DspFile() function.

This is a limitation of the DspFile() cicode function that the maximum file size of the text file that it can open is 1 MB.
An alternative approach is to use the CiText.Textbox ActiveX control that comes with VJC. Not only can it display large
files, it’s look and feel is customizable.
Was this helpful?
What can we do to improve the information ?