Technical FAQs

Ask a Question

We need to move the tag values from one IODevice to other IODevice, is there any cicode or functions available for this operation.

For writing tags values from one IO Device to another IO device is possible with a simple cicode using a equal sign like as in below cicode :
FUNCTION TagUpdate( )
Dev1_Tag1 = Dev2_Tag1 ;
Dev1_Tag2 = Dev2_Tag2 ;
This will move tag values of Dev2_Tag1 and Dev2_Tag2 in Dev1 tags.
Also you need to make sure that you will call this function in events every second.
Was this helpful?
What can we do to improve the information ?