Technical FAQs

Ask a Question

Can we have password protection of Vijeo Citect Project.

You cannot protect your project with password in your system. Only backup of the project you can put password protected, while taking
backup from the system with the help of “Use Encryption” field and to restore the backup you have to enter the correct password.
Was this helpful?
What can we do to improve the information ?