Technical FAQs

Ask a Question

An OPC Client can browse and add tag items from a single cluster project successfully running on a SCADA machine, however it's not possible with a multi-cluster project.

This occurs in SCADA V 7.20 (and previous versions). To resolve this, add a cluster name manually as a prefix to tags
in the OPC client (e.g. ClusterName.TagName) for tag communication with SCADA OPC Server.
Was this helpful?
What can we do to improve the information ?