Technical FAQs

Ask a Question

How many BMXERT1604T modules are supported per Modicon X80 drop.

Modicon X80 drop supports a maximum of 36 expert channels, BMXERT1604T module contains 4 expert channels. so
it supports a maximum of 9 nos. of BMXERT1604 T modules if there is no other expert module placed in the drop.
Was this helpful?
What can we do to improve the information ?