Technical FAQs

Ask a Question

Can I transfer PLC application program from PC to PLC using Unity loader software.

The Unity Loader software provides the following transfer features:
  • Transfer of a Unity Pro application from a PC to a Modicon M340, Premium or Quantum PLC.
  • Transfer of a Unity Pro application from a Modicon M340, Premium or Quantum PLC to a PC.
  • Transfer of firmware (FW) from a PC to a Modicon M340 PLC or to a module with firmware of the Modicon M340 platform.
Note: The Unity Loader software requires one of the following operating systems:
  • Microsoft Windows XP Professional
  • Microsoft Windows Vista Business
  • Microsoft Windows 7 Professional
Was this helpful?
What can we do to improve the information ?