Technical FAQs

Ask a Question

What is the maximum loop resistance for each 140ACO13000 output.

The equation for max field resistance = (loop power supply voltage - min ACO output voltage(6V) ) / max output current (25mA).
 
Example with 24VDC: (24-6)/25 = 720 Ohms
Was this helpful?
What can we do to improve the information ?