Technical FAQs

Ask a Question

What is the component required when we need to connect the Varlogic NRC12 to Modbus RS485 communication link.

52451 is required to order. 52451 reference includes one CCA (Controller Communication Adapter, fiber output module for PFC) and
one MCU (Modbus Coupler Unit, RS-485 adapter for fiber or RS-232) including the fiber optic cable is connected the CCA and the
MCU to connect the Varlogic NRC12 to Modbus RS485 communication link.
Was this helpful?
What can we do to improve the information ?