Technical FAQs

Ask a Question

How to connect Controller Communication Adapter to NRC12 Varlogic controller.

Installing procedure for CCA (Controller Communication Adapter)
 
1. Remove the cover of the connector
2. Slide the CCA into the connector track
3. Check that the CCA is properly installed
4. Remove the protect plugs and connect the fiber cable
 
See the attached picture installing procedure for CCA
Was this helpful?
What can we do to improve the information ?