Technical FAQs

Ask a Question

What is an external temperature sensor for NRC12 Varlogic controller and its part reference number.

The controller has terminals T1/T2 for external temperature sensor. With the external temperature probe the
temperature in a critical point in a capacitor bank can be monitored with the controller.
 
The External Temperature Sensor can be purchased as an option and installed into the capacitor bank. The catalogue r
eference for Temperature external probe for NRC12 is 52452.
Was this helpful?
What can we do to improve the information ?