Technical FAQs

Ask a Question

What is the limit on Modbus multi drop connection for both the HMI port and also on the Modbus option in TeSys T relay.

The limit on the left or the right port for TeSys T Modbus product is the same.
These features are defined by Modbus standard: Maximum 1000 meters without repeater and 31 maximum slaves.
Was this helpful?
What can we do to improve the information ?