Technical FAQs

Ask a Question

Is is possible to use TeSys T relay for single phase motor application.

Yes. There is a configuration for single phase is available, you need to download the same from Powersuite software.
 If single phase is selected, use the two outer (Left and Right) connection terminal for the power cable.
Was this helpful?
What can we do to improve the information ?