Technical FAQs

Ask a Question

What Type of RTD's are supported with the Sepam relays.

The Sepam relays support the following three types of RTD's (this only applies to Sepam relays that support the MET148-2 module):
 
1. PT100 (Platinum 100 ohm)
2. NI100 (Nickel 100 ohm)
3. NI120 (Nickel 120 ohm)
 
Note: The MET148-2 (RTD Module for the Sepam relays) only supports three wire RTD's. This does not mean two wires and a shield.
Was this helpful?
What can we do to improve the information ?