Technical FAQs

Ask a Question

How do I wire or configure the LED's on a Sepam relay.

The LED's on the Sepam relay are internal to the unit and do not need wiring. They may be configured via the SFT2841
software either in the individual protection screens or the control matrix.
Was this helpful?
What can we do to improve the information ?