Technical FAQs

Ask a Question

How to clear alarms using the front display for a Sepam relay.

To clear the alarms from the front screen:
1. Press the button with the triangle with ! in the center
2. Highlight List (defaulted to this) using the up or down arrow key
3. Press the reset (enter) key
4. Press the clear button
Note: This will clear the most recent four alarms; if more alarms are present the list and details options will still be
available in the alarm screen. If all of the alarms have been cleared, only list will be available. 
Was this helpful?
What can we do to improve the information ?